AXIS#.BODE.PRBDEPTH
Description
AXIS#.BODE.PRBDEPTH sets the length of the PRB signal before it repeats. This applies only when AXIS#.BODE.MODE = PRB. The PRB excitation will repeat after (2^AXIS#.BODE.PRBDEPTH) / AXIS#.BODE.EXCITEGAP drive samples.
Example
Code
Set AXIS1.BODE.PRBDEPTH to 19:
--> AXIS1.BODE.PRBDEPTH 19
Get AXIS1.BODE.PRBDEPTH (already set to 19):
--> AXIS1.BODE.PRBDEPTH 19
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
NA |
|
Range |
4 to 19 |
|
Default Value |
19 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.BODE.PRBDEPTH | 0x5001 | 0x2 | USINT | - | - | RW | False |
| AXIS2.BODE.PRBDEPTH | 0x5101 | 0x2 | USINT | - | - | RW | False |